ALWAYS DOWNLOAD THE LATEST VERSION OF REVIT CONTENT BEFORE USING THEM IN A NEW PROJECT.

This change history file can be used to help you determine whether or not the changes
in the latest version available warrant the effort to update a family that is already
being used in an existing project.

Family file Dates:  2022 January 3
  - Taken refrigerant lbs out of txts

Family file Dates:  2020 August 28
  - Updated the SA and RA dimensions and locations per the DST drawings for size 3-5 Maverick I bottom discharge units

Family file Dates:  2018 December 4
  - Fixed the condensate drain location for size 7-12 Maverick I bottom discharge units

Family file Dates:  2018 May 9
  - Added newly designed units for size 7-12 Maverick I bottom discharge units


Family file Dates:  2016 January 22
  - Added support for size 61-75 Maverick II bottom discharge units


Family file Dates:  2015 October 15
  - Added support for size 26-50 Maverick II side discharge units


Family File Dates: 2013 October 1
  - Rebranded to Daikin Applied

Family file Dates:  2012 March 12
  - Added support for size 26 Maverick II units


Family file Dates:  2011 November 8
  - Fixed Product Page URL to redirect verbiage on both I & II's


Family file Dates:  2011 July 15
  - Released 4 Maverick II side discharge units



Family file Dates:  2011 February 28
  - Fixed curb visibility issue on one Maverick I file
  - Fixed base rail color on 3 Maverick II files



Family file Dates:  2011 February 23
  - Added support to the Maverick II families for the new Enthalpy Wheel feature in these products
      - Toggle it on or off with the "Enthalpy Wheel" instance parameter in the Construction group



Family file Dates:  2010 November 2
  - Reduced nested family usage even more, making the files even smaller
  - Added new parameters to the Construction group to control hood options
  - Easier to use:  Significantly simplifyied type catalogs
  - Made file names more intuitive, using "BtmDischarge" and "SideDischarge" to describe connectors



Family file Dates:  2010 August 19
  - Further reduced nested family usage and simplified geometry to decrease the file sizes even more
  - Assembly Code values are now compliant with MasterFormat 2010 (can be helpful for e-SPECS users)
  - Cleaned up the floor plan view
  - Removed 7.5 ton 1 compressor from all type catalogs Air_Conditioner-Packaged_Rooftop-McQuay-(6-12.5_Ton)-(MPS_Maverick_I)
    - No longer supported 



Family file Dates:  2010 July 16
  - Reduced nested family usage to decrease the file sizes
  - Improved documentation links for longer life expectancy



Family File Dates: 2010 June 23
  - Removed the triangular void from the condenser section on Maverick II families, to simplify the model




Family File Dates: 2010 May 21

  - Upgraded to Revit 2010 format.  Changes include:
    - OmniClass value added
    - Defined exactly one type in the family, to help indicated if the Type Catalog wasnt used properly:
            "INVALID TYPE - Use Load Family and Type Catalog Instead"
    - Clearance volume changed to green (easier to see in Revit interference checks)
    - Set materials "Render Appearance" settings to create better images when the model is rendered
    - Material names better conform to the Revit Model Content Style Guide
    - Product Page URL parameter added for conformance to the Revit Model Content Style Guide
    - "URL" parameter value conforms better to Revit Model Content Style Guide 
    - To reduce load on Revit, web link parameters were changed to Type parameters
    - To improve usage for system design purposes, parameters such as those for capacities, temperatures, power values and others were changed to Instance parameters